Deltag i the Arla Protein Padel League med GHS Padel - Join GHS Padel for the Arla Protein Padel League

Kære Padelspillere,

Vi i GHS Padel Komitéen er glade for at kunne meddele, at vi har fået midler til at deltage i Arla Protein Padel Ligaen med to hold af 6 deltagere.

Turneringen består af fem spilledage plus en play-off dag til finalerne. Spilledagene kræver mindst fire spillere, og tiden kan fastsættes af hvert hold for hver kamp individuelt, så det er muligt at passe ind i alle skemaer!

Vi vil tilmelde begge hold i 4. division, som er padelniveau op til 3, og have hjemmebane i Bjerringbro Padel Center. Al information om Arla Protein Padel Ligaen kan findes her: https://padelidanmark.dk/turneringer/arla-protein-ligaen-foraar-sommer-2025/

De 12 pladser på de to hold vil blive fyldt efter først-til-mølle-princippet.

Kontakt venligst Mads Enggrob Nymann – Mnymann@Grundfos.com, hvis du er interesseret.

Med venlig hilsen
GHS Padel

Dear Padel Players,

We in the GHS Padel Committee are excited to announce that we got funds to participate in the Arla Protein Padel League with two teams of 6 participants.

The tournament consists of five game days plus a play-off day for the finals. The game days requires a minimum of four players and the time can be set by each team for each game individually, so it is possible to fit into all schedules!

We will sign both teams up in 4th division which are padel levels up to 3 and have a home court in Bjerringbro Padel Center.
All information regarding Arla Protein Padel League can be found here:
https://padelidanmark.dk/turneringer/arla-protein-ligaen-foraar-sommer-2025/

The 12 spots on the two teams will be filled on a first come first serve basis.

Please Reach out to Mads Enggrob Nymann – Mnymann@Grundfos.com if you’re interested.

Best Regards
GHS Padel