GHS Games Volley - King and Queen of Court vindere/winners

For allerførste gang og som en del af GHS Games 2025 har volleyball kåret Queen and King of Court.

Mange dygtige spillere mødte op to oktober-tirsdage i Grundfos hallen og dystede om de ærefulde titler.

Efter mange intense kampe og med spænding til det sidste blev det Henriette Drægert Grønning og Adam Schwarz, som løb med de flotte titler. De er begge rutinerede spillere og medlemmer af GHS volleyball, og de kan nu se frem til at modtage deres velfortjente præmier og kalde sig Queen and King of Court indtil næste GHS Games. Stort tillykke til de to vindere.

GHS volleyball, Heidi Lassen

For the very first time and as part of the GHS Games 2025, volleyball has crowned a Queen and King of Court.

Many skilled players turned up on two October Tuesdays in the Grundfos hall and competed for these prestigious titles.

After many intense matches and excitement until the very end, it was Henriette Drægert Grønning and Adam Schwarz who claimed the impressive titles. Both are experienced players and members of GHS volleyball, and they can now look forward to receiving their well-deserved prizes and calling themselves Queen and King of Court until the next GHS Games. Congratulations to the two winners.

GHS volleyball, Heidi Lassen